Unknown byte received from Tag when reading max mailbox size.
Hi,
I'm using an ST25DV64KC tag to communicate with an Android app using the st25 sdk and the Mailbox. The problem arises when the app reads a message of the maximum mailbox capacity. In that case, an 0xE4 character appears as the last character but I'm pretty sure the firmware didn't put it.
Here is an example of an interaction
2025-05-12 08:32:09.466 12263-19515 Iso15693CustomCommand com.wavecontrol.mtiotmobileapp D ==> Send readMsgLength command: 22 ab 02 7f 46 b6 7c 67 51 02 e0
2025-05-12 08:32:09.480 12263-19515 Iso15693CustomCommand com.wavecontrol.mtiotmobileapp D Response: 00 ff
2025-05-12 08:32:09.483 12263-19515 Iso15693CustomCommand com.wavecontrol.mtiotmobileapp D ==> Send readMsg command: 22 ac 02 7f 46 b6 7c 67 51 02 e0 00 ff
2025-05-12 08:32:09.588 12263-19515 Iso15693CustomCommand com.wavecontrol.mtiotmobileapp D Response: 00 02 7b 22 6a 73 6f 6e 72 70 63 22 3a 22 32 2e 30 22 2c 22 72 65 73 75 6c 74 22 3a 22 54 30 36 3a 31 34 3a 34 35 2e 33 30 36 20 52 65 63 65 69 76 65 64 20 67 65 74 5f 69 6e 66 6f 5f 6d 65 61 73 75 72 65 5c 6e 5b 49 5d 20 32 30 32 35 2d 30 35 2d 31 32 54 30 36 3a 31 34 3a 34 38 2e 37 32 31 20 4e 46 43 20 73 65 73 73 69 6f 6e 20 73 74 61 72 74 5c 6e 5b 49 5d 20 32 30 32 35 2d 30 35 2d 31 32 54 30 36 3a 31 34 3a 34 38 2e 37 32 32 20 52 65 73 74 61 72 74 65 64 20 6f 6e 65 2d 73 68 6f 74 20 74 69 6d 65 72 20 4e 46 43 20 73 65 73 73 69 6f 6e 20 74 69 6d 65 72 20 77 69 74 68 20 74 69 6d 65 6f 75 74 20 31 30 30 30 30 20 6d 73 2e 5c 6e 5b 49 5d 20 32 30 32 35 2d 30 35 2d 31 32 54 30 36 3a 31 34 3a 34 38 2e 37 32 37 20 52 65 63 65 69 76 65 64 20 67 65 74 5f 69 6e 66 e4
As can be seen, the retrieved message length is 255, which according to the datasheet is the size of the message in the mailbox - 1.

Then I issue a readMsg command passing it the 0xff, so it should read 0xff + 1 bytes

But at the end I get that 0xe4, which I'm confident wasn't put by the host side. As a result I lose one byte.
That doesn't seem to happen when writing less than 256 bytes.
Where that character may come from? I've tried putting several different messages in the mailbox but the last character is always 0xe4.