Skip to main content
PGama.1
Associate
August 19, 2021
Question

Can STM32H7 chip be directly program with STLink/V2 via SWD ?

  • August 19, 2021
  • 7 replies
  • 4393 views

I have designed a costimazed PCB board based on NECLEO-H743Z12 board, and I have removed the build in STLink debugger, hoping that I will use the external STLink/V2 programmer via SWD. I have followed the schematics data sheet and connected pins [3.3V, GND, TMS, TCK, SWO] directly to H7 chip pins [PA13, PA14, PB3, VDD,GND]. I’m using the STLink software tool to detect the chip but till now I’m constantly getting error messages that the target chip is not detected.

What am I missing, am I doing something wrong ? Is it possible to program this chip directly? and how ? I will really appreciate your help as I’m new and this is my first customize design.

thanks !

7 replies

Tesla DeLorean
Guru
August 19, 2021

It should be capable of working and connecting. I'd have the NRST wired up also.

That you can't connect is more indicative that the H7 isn't running.

What other signs-of-life testing have you done? Can you pull BOOT0 High and connect to the ROM System Loader via USART1 (PA9,PA10) or USB?

Check level on NRST pin.

Check voltage on VCAP pins.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
PGama.1
PGama.1Author
Associate
August 19, 2021

Hi @Community member​ thanks for your quick response, I forgot to mentioned that NRST PIN was connected. I have attached the schematics bellow. the only test I did was to check the VDD powering the board with 3.3V and i have tested the VCAP pins with 1V, as for the USART, only the USART3 pinout is available on this breakout board.

0693W00000DplLZQAZ.png

EZHON.1
ST Employee
March 17, 2025

Do you use the standard debugging tool (external STLink/V2 programmer). The SWD Programmer connector from schematic isn't the stardard one.

PGama.1
PGama.1Author
Associate
August 19, 2021

Update on the current issue (STM32H7 STlink-v2 programmer to breakout board ). it seems i can connect but the chip is not responding. here is the results from the STlink software tool. What am i missing ?

0693W00000DpuudQAB.png 

And the next is the results from the cubeIED

 0693W00000DpumpQAB.png

Visitor II
March 16, 2025

Hi, is this resolved? I am facing same issue.

Tesla DeLorean
Guru
March 16, 2025

Then probably something wrong with your design, try presenting details of that..

Perhaps power issues, or correct part orientation. 

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
Visitor II
March 16, 2025

STM32H745ZI, I am using stm32 v2 for swd connections. The core is powered through SMPS, I am getting 1.2V at VDDLDO.

Lead II
March 17, 2025

Do you have configured the proper SMPS settings in STM32CubeMX?

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
Visitor II
March 17, 2025

I am first trying to connect it to stm32 cube programmer

Lead II
March 17, 2025

Have you tried connecting under reset?

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
Lead II
March 21, 2025

it can help to give a power cycle while holding the reset and then connecting under reset

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
Visitor II
March 21, 2025

I am now able to connect to the target, found out my debugger is faulty. But, still facing problem after programming the controller. The program is simple LED toggle. I have checked the power supply configuration HAL_PWREx_ConfigSupply(PWR_DIRECT_SMPS_SUPPLY); The MCU is getting connected only when Boot0=1 after programming it got disconnected. Attached the log of cubeprogrammer.

Lead II
March 21, 2025

Where did you set your first breakpoint?

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
Visitor II
March 21, 2025

There is no breakpoint in the code

Lead II
March 21, 2025

Add a breakpoint as early in the code as possible. In SystemInit. And then step through the code.

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."