Can't access STM32-LPM01-XN via terminal after firmware update to v1.0.8
I’m using the X-NUCLEO-LPM01A (PowerShield) and previously had firmware version 1.0.1, where I could connect via a serial terminal over USB and interact with the board using commands.
But error occured short after, with LED 2 on the board indicating USB enumeration failure.
Updating the STM32-LPM01-XN firmware version to the latest one (1.0.8) solved that issue but now no sign of connection via a COM port terminal.
Everything works fine using via a graphical user interface using the STM32CubeMonitor-Power software tool.
But would prefer controlling via COM terminal ...
Thanks for the support