Skip to main content
Associate II
March 5, 2025
Question

Can't initialize SDMMC on stm32h757i-eval

  • March 5, 2025
  • 2 replies
  • 490 views

Hello,

I am using a STM32H757-i eval board. 

I created a project through file >> new stm32 project, selected my board, then generated code.

However, I am going into error handler when initializing the SDMMC.

 

My path to go to error handler :

 

 MX_SDMMC1_SD_Init();
 if (HAL_SD_Init(&hsd1) != HAL_OK)
 {
 Error_Handler();
 }
 /* Initialize the Card parameters */
 if (HAL_SD_InitCard(hsd) != HAL_OK)
 {
 return HAL_ERROR;
 }
 errorstate = SD_PowerON(hsd);
 if (errorstate != HAL_SD_ERROR_NONE)
 {
 hsd->State = HAL_SD_STATE_READY;
 hsd->ErrorCode |= errorstate;
 return HAL_ERROR;
 }
 errorstate = SDMMC_CmdGoIdleState(hsd->Instance);
 /* CMD8: SEND_IF_COND: Command available only on V2.0 cards */
 errorstate = SDMMC_CmdOperCond(hsd->Instance);
 errorstate = SDMMC_GetCmdResp7(SDMMCx);
uint32_t SDMMC_GetCmdResp7(SDMMC_TypeDef *SDMMCx)
{
 uint32_t sta_reg;
 /* 8 is the number of required instructions cycles for the below loop statement.
 The SDMMC_CMDTIMEOUT is expressed in ms */
 uint32_t count = SDMMC_CMDTIMEOUT * (SystemCoreClock / 8U / 1000U);

 do
 {
 if (count-- == 0U)
 {
 return SDMMC_ERROR_TIMEOUT;
 }
 sta_reg = SDMMCx->STA;
 } while (((sta_reg & (SDMMC_FLAG_CCRCFAIL | SDMMC_FLAG_CMDREND | SDMMC_FLAG_CTIMEOUT)) == 0U) ||
 ((sta_reg & SDMMC_FLAG_CMDACT) != 0U));

 if (__SDMMC_GET_FLAG(SDMMCx, SDMMC_FLAG_CTIMEOUT))
 {
 /* Card is not SD V2.0 compliant */
 __SDMMC_CLEAR_FLAG(SDMMCx, SDMMC_FLAG_CTIMEOUT);

 return SDMMC_ERROR_CMD_RSP_TIMEOUT;
 }

So having SDMMC_ERROR_CMD_RSP_TIMEOUT as error.

 

I tried both of theses solutions, both didn't work :

https://community.st.com/t5/stm32-mcus-embedded-software/stm32h757i-eval-sd-card-does-not-seem-to-be-recognized/m-p/151848#M8777

https://community.st.com/t5/stm32-mcus-products/stm32h757i-eval-sdmmc-initialization-problem/m-p/707296#M257413

Would you have ideas to debug it ?

Best Regards

Matteo

2 replies

Andrei Chichak
Lead
March 5, 2025

@Matteo-uC what firmware are you using? (Project Manager, Project, Mcu and Firmware Package)

I'm having a very similar issue with a U5 processor, the issues may be connected.

Andrei Chichak
Lead
March 7, 2025

Please check the peripheral clock enable bit for SDMMC1 in RCC AHB3ENR. If it is 0, the clock isn't turned on to the device.

I saw this on another family where the wrong SDMMC was being enabled in HAL_SD_MspInit.