Question
ADC Error : only returns '0X01AF'
I'm using stm32c011f4u6 and keil5. and I'm using 2 ADC channels by Polling.
Every time I read an ADC channel, it only return '0X01AF'. This is the same for both channels,
even if I remove one channel and read it again with only one channel used, the same problem appears.
static void ADC_Init(void)
{
ADC_ChannelConfTypeDef sConfig = {0};
//!!! HAL_ADC_Init is commented because some parameters are missing
hadc.Instance = ADC1;
hadc.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV1;
hadc.Init.Resolution = ADC_RESOLUTION_12B;
hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc.Init.ScanConvMode = ADC_SCAN_ENABLE;
hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc.Init.LowPowerAutoWait = DISABLE;
hadc.Init.LowPowerAutoPowerOff = DISABLE;
hadc.Init.ContinuousConvMode = DISABLE;
hadc.Init.NbrOfConversion = 1;
hadc.Init.DiscontinuousConvMode = DISABLE;
hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc.Init.DMAContinuousRequests = DISABLE;
hadc.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc.Init.SamplingTimeCommon1 = ADC_SAMPLETIME_1CYCLE_5;
hadc.Init.SamplingTimeCommon2 = ADC_SAMPLETIME_1CYCLE_5;
hadc.Init.OversamplingMode = DISABLE;
hadc.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
if(HAL_ADC_Init(&hadc) != HAL_OK)
{
Error_Handler();
}
while(HAL_ADCEx_Calibration_Start(&hadc) != HAL_OK);
}
uint16_t NTC1_Read(void)
{
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_14, GPIO_PIN_SET);
ADC_ChannelConfTypeDef sConfig = {0};
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
if(HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_2;
sConfig.Rank = ADC_RANK_NONE;
sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
if(HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
Error_Handler();
}
HAL_ADC_Start(&hadc);
HAL_ADC_PollForConversion(&hadc, HAL_MAX_DELAY);
ADC_CH1 = HAL_ADC_GetValue(&hadc);
HAL_ADC_Stop(&hadc);
CH1 = 3000 * ADC_CH1 / 4096;
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_14, GPIO_PIN_RESET);
return CH1;
}
uint16_t NTC2_Read(void)
{
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_15, GPIO_PIN_SET);
ADC_ChannelConfTypeDef sConfig = {0};
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = ADC_RANK_NONE;
sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
if(HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_2;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
if(HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
Error_Handler();
}
HAL_ADC_Start(&hadc);
HAL_ADC_PollForConversion(&hadc, HAL_MAX_DELAY);
ADC_CH2 = HAL_ADC_GetValue(&hadc);
HAL_ADC_Stop(&hadc);
CH2 = 3000 * ADC_CH2 / 4096;
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_15, GPIO_PIN_RESET);
return CH2;
}
These are my ADC functions. What's wrong with this program?