Skip to main content
Associate
February 1, 2024
Question

CPU is getting stuck in HAL_GetTick() for any example project/application on STM32H750B-DK

  • February 1, 2024
  • 6 replies
  • 2459 views

Hello,

we are using STM32CubeIDE v1.14 & STM32Cube_FW_H7_V1.11.0 for STM32H750B-DK discovery kit.

whenever we try to flash any application (LTDC_Paint) or GPIO_Toggle or any example project, binary is getting flashed but CPU is getting stuck in HAL_GetTick() in MT48LC4M32B2_Delay() function always when we try to debug the firmware using on-board STLINK.

Please suggest way forward to resolve this issue.

Thanks,

Satya Sudhir

6 replies

TDK
Super User
February 1, 2024

Go into your system_stm32h7xx.c file and uncomment the line with the following:

#define USER_VECT_TAB_ADDRESS
"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
February 5, 2024

Hi @TDK,

There is no such macro "USER_VECT_TAB_ADDRESS" in the project.

Below are the macros that are disabled by default in system_stm32h7xx.c:

 

/************************* Miscellaneous Configuration ************************/

/*!< Uncomment the following line if you need to use external SDRAM mounted

on DISCO board as data memory */

/*#define DATA_IN_ExtSDRAM*/

 

/*!< Uncomment the following line if you need to use initialized data in D2 domain SRAM */

/* #define DATA_IN_D2_SRAM */

 

/*!< Uncomment the following line if you need to relocate your vector Table in

Internal SRAM. */

/* #define VECT_TAB_SRAM */

#define VECT_TAB_OFFSET 0x00000000UL /*!< Vector Table base offset field.

This value must be a multiple of 0x200. */

/******************************************************************************/

 Please suggest way forward.

May I know the reason why tick is not getting incremented in the default SDK project (without any changes) ?

Thanks,

Satya Sudhir

TDK
Super User
February 5, 2024

Oh, this is an example project. Hmm, not sure. They should be working. Certainly GPIO_Toggle should be simple enough to go through and debug. Or creating a new project from CubeMX and testing HAL_Delay would be informative.

"If you feel a post has answered your question, please click ""Accept as Solution""."
mƎALLEm
Technical Moderator
February 5, 2024

Hallo,

That's strange.

Any example provided in STM32CubeH7 should work without any modification.

Are you sure the board you are using were not modified? Did you test with a second board?

At least GPIO_Toggle example should work.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
Visitor II
July 7, 2024

I'm having exactly the same issue with the same board, but with a newer firmware version, STM32Cube_FW_H7_V1.11.2

This is the call stack:

jrrossi_0-1720374885458.png

The example is being build without any modification.

Ayoub Cheggari
Senior
July 9, 2024

Hi,

Can you try lower the SysTick priority to 0 and other to > 1?

AyoubCheggari_0-1720538975949.png

 

That might work as it works for me!

Ayoub

Visitor II
July 9, 2024

The BSP project for the STM32H750B-DK kit doesn't come with a .ioc file.

I changed the SysTick interrupt priority to 0, but still hanging on the HAL_Delay.

It's just really weird, the most basic demo project of the kit simply does not work out of the box.

If even the ST engineers struggle to get this kit running, how am I supposed to learn how to use it?

Ayoub Cheggari
Senior
July 10, 2024

So you have SysTick interrupt priority set to 0 and all others > 1? can you please make a screenshot of your NVIC config?

Visitor II
July 11, 2024

As I said, the BSP project does not come with an .ioc file, so I can't configure it with MX.

What I did was:

jrrossi_0-1720715409307.png

still no luck...

If I start a new project using MX, the systick works fine, so I'm sure the board is not defective.