Skip to main content
Visitor II
February 12, 2025
Question

Current measurement in STM32N6570-Discovery Kit

  • February 12, 2025
  • 1 reply
  • 938 views

Hello,

I am currently using STM32N6657XOHXQ(Discovery Kit), I am currently running UART_HyperTerminal_IT example given in CubeMX Example. I need to measure the current consumption by board for that. I have removed Resistor (R31)  as

Tirth_1-1739345776928.png

 

Tirth_0-1739345007939.png

For external SMPS Output power mode, and my assumption is that after removing resistor and placing current measurement device between 3 and 4 pin of CN2 connector the current should be measured and prints should start but when i remove Current measurement device from the loop, the prints should be stopped as the path will be open. Still i am getting the print on console. Can you please prove the detailed steps to measure current consumption of the MCU Core.

1 reply

RomainR.
ST Employee
February 13, 2025

Hello @Tirth 

Refer to MB1939-N6570-C02 Board schematic in page 5. 

https://www.st.com/en/evaluation-tools/stm32n6570-dk.html#cad-resources:~:text=MB1939%2DN6570%2DC02%20Board%20schematic

In addition to desoldering R31, there is a series shunt resistor R35.

The VDDCore current measurement method on CN2 between pin 3 and 4, must be done through the 50mΩ R35 shunt resistor with a voltmeter measuring the voltage drop. The current can then be determined by Iddcore = VDDCore / R35. Do not use an ampere meter.
VDDCore depends on the configuration of the external DC-DC U2 (TPS62088YFP). Either 0.81V in VOS_NOMINAL or 0.89V in VOS_OVERDRIVE by the state of GPIO PF4. By default, PF4=Low, VDDCore is set to VOS_NOMINAL 0.81V and the STM32N6 CPU frequency is set to 600MHz.

Let me know if it helps?
Best regards,

Romain,

 

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.