Skip to main content
FJB2069
Senior
May 13, 2025
Solved

custom stm32F746 board with 5" LCD - choosing lcd panel

  • May 13, 2025
  • 1 reply
  • 363 views

Looking for some input for selecting an lcd for my custom stm32F764 application.

Currently I have the LCD that came with the stm32F746G-DISCO board working with my custom board.

The "DISCO" lcd is 4.3: capacitive 480x272.  I need a 5" resistive LCD.  

I think I have the resistive aspect figured out, but most of the 5" LCD's are 800x480. 

1) I need to verify I will not have a memory issue going with higher res lcd.  What is the best way to determine this?

2) The controller on the DISCO LCD is an ST7282,  Do I need to make sure the 5" LCD I pick uses a similar controller? If not, will I be re-writing a lot of driver code to get it to work?

3) should I make sure display has same 40 pin connector with same signals,  seems like there is typically a 40 or 50 pin option.  (I will most likely have a separate connector for the 4 pin resistive panel)

 

Just need some advice on this as I do not have much experience with using different TFT displays in custom applications!

Best answer by EZHON.1

Hello,

If you want to customize your LCD, you can contact the LCD Vendor directly. Liking http://www.lcdlcm.com, which vendor support our STM32 boards.

B.R

Eric

1 reply

EZHON.1
EZHON.1Best answer
ST Employee
May 15, 2025

Hello,

If you want to customize your LCD, you can contact the LCD Vendor directly. Liking http://www.lcdlcm.com, which vendor support our STM32 boards.

B.R

Eric