Skip to main content
Associate II
July 16, 2024
Question

Debugging STM32F103C8T6 using the debugger of STM32F446RE nucleo board.

  • July 16, 2024
  • 2 replies
  • 1259 views

Hii everyone,

I want to debug STM32F103C8T6 controller by using the debugger present in the STM32F446RE nucleo board. After setting the parameters , when i go for debugging the following error is coming. Please guide me how i could debug my respective code using the STM32F103C8T6 controller.

Output

STMicroelectronics ST-LINK GDB server. Version 7.7.0

Copyright (c) 2024, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

 

Device connect error

 

Error in initializing ST-LINK device.

Reason: Failed to connect to device. Please check power and cabling to target.

 

Thank You...

2 replies

Technical Moderator
July 16, 2024

Hello @Shaku ,

Make sure to upgrade ST-Link firmware.

Check the debug pins connections and GPIO pin used for toggling.

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
ShakuAuthor
Associate II
July 16, 2024

Thank you !!!!

After checking the debug pins and GPIO pin i am getting the same error. I'm also upgrading the ST-Link firmaware but the error is coming continuously.

Andrew Neil
Super User
July 16, 2024

@Shaku wrote:

I want to debug STM32F103C8T6 controller by using the debugger present in the STM32F446RE nucleo board


Have you set all the links on the Nucleo board correctly - to disconnect the STM32F446RE Target from the ST-Link?

Post a schematic of your connections.

Post some good, clear photos of your setup.

 


@Shaku wrote:

 

Error in initializing ST-LINK device.


That means the computer isn't even connecting to the ST-Link.

Does it show up in the Device Manager (or equivalent)?

AndrewNeil_0-1721121256487.png

If not, check your cable: are you sure it's a full data cable - not jus a charging cable?

Try other cables.

Try other USB ports.

 

Knowledgebase article:

https://community.st.com/t5/stm32-mcus/how-to-solve-debugger-connection-issues/tac-p/698105#M956

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ShakuAuthor
Associate II
July 17, 2024

Thank you!!!

I am using it in Linux(ubuntu) OS.

this is the circuit connection of STM32F103C8T6 with STM32F446RE nucleo board debugger.this is the circuit connection of STM32F103C8T6 with STM32F446RE nucleo board debugger.