Driving 11 LPS27HHTW sensors on a single I3C bus
Hello everyone,
I need to drive up to 11 LPS27HHTW pressure/temperature sensors using an STM32C5 microcontroller. Currently, I'm testing the setup on an NUCLEO-C562RE board with multiple STEVAL-MKI220V1 modules.
At first glance, using I3C dynamic addressing seemed to solve the bus conflict issue. However, while testing, I realized that all of these sensors share the exact same 48-bit PID (0x020800B30000). This generates a collision when doing an ENTDAA broadcast.
Since the sensors only have 2 possible static I2C addresses (0x5c and 0x5d, depending on the SA0 pin level), I cannot use the SETDASA command for all 11 devices either.
I can't split the sensors across different buses since there are too many of them. I would like to know if there are better architectural options than playing with the CS pin levels using 11 dedicated GPIOs to enable/disable communication on each sensor individually.
Any advice on how you would drive that many sensor using a STM32C5 mcu?
Best regards,
Mathias