Skip to main content
Associate
September 3, 2024
Solved

Error: Connection to target must be established before performing the erase command.

  • September 3, 2024
  • 2 replies
  • 1793 views

Hi, 

I have an issue on STM32H7B3I-DK, I am not able to flash code, I atleast want to perform full erase, but I am getting " Error: Connection to target must be established before performing the erase command." error.

Isy777_0-1725376402941.png

Fig: STM32CubeProgrammer.

Isy777_1-1725376472561.png

Fig: Trying to erase the board. But still getting the above error.

Anything else can I do on this board.

 

Best answer by mƎALLEm

Ok what about my second point? :

"If not, could be something related to a wrong power configuration you set previously in your application. The board is wired in SMPS by default. So if you set LDO in your application you lose the connection.

Please see this thread."

2 replies

Andrew Neil
Super User
September 3, 2024

It's telling you that it can't connect to the Target; therefore it won't be able to do anything to the Target until that is fixed!

AndrewNeil_0-1725377012258.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
Technical Moderator
September 3, 2024

Hello,

Are you sure you are using a data cable and not a charging cable?

If not, could be something related to a wrong power configuration you set previously in your application. The board is wired in SMPS by default. So if you set LDO in your application you lose the connection.

Please see this thread.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
Andrew Neil
Super User
September 3, 2024

@mƎALLEm wrote:

Are you sure you are using a data cable and not a charging cable?


It seems to be indicating that the connection to the ST-Link is OK:

AndrewNeil_0-1725377413248.png

So the cable must be good?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Isy777Author
Associate
September 3, 2024

Yeah, Cable is good. Something must be done at board's end.