Skip to main content
Associate
January 27, 2025
Solved

net SHIELD industrial ethernet protocols expansion board

  • January 27, 2025
  • 2 replies
  • 783 views

Hello STM Community,

I'm working on netSHIELD ethernet protocols expansion board from HilScher, In the product details they have told 

Supported Devices STM32F4,STM32F7

Does it mean I can not use any other STM32 MCU with this netSHIELD industrial ethernet protocols expansion board
I want use STM32H753 because I need 9 UART and this MCU has it.

moneshrathod_0-1737973231446.png

 

Best answer by mƎALLEm

Hello @moneshrathod and welcome to the community.

Only F4 and F7 products are supported but as the solution was developed by Hilscher (an ST partner) you can contact them directly over this link.

2 replies

Andrew Neil
Super User
January 27, 2025

@moneshrathod wrote:

Does it mean I can not use any other STM32 MCU with this netSHIELD industrial ethernet protocols expansion board


Almost certainly not - just that those are the MCUs for which ST provide ready-to-go examples.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate
January 27, 2025

Its still not clear. Can I use STM32H753 and put bin flash file of STM32F7 in STM32H753 

 

mƎALLEm
Technical Moderator
January 27, 2025

@moneshrathod wrote:

Its still not clear. Can I use STM32H753 and put bin flash file of STM32F7 in STM32H753 

 


No.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
mƎALLEm
mƎALLEmBest answer
Technical Moderator
January 27, 2025

Hello @moneshrathod and welcome to the community.

Only F4 and F7 products are supported but as the solution was developed by Hilscher (an ST partner) you can contact them directly over this link.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."