No external UART RX signal
Reference
- Board: Nucleo-H753ZI (MB1364, ST-LINK V3, rev B)
Summary
We have an external UART sensor (WitMotion HWT9053 IMU) connected to the Arduino D0/D1 header pins on a Nucleo-H753ZI. The sensor is confirmed working on Arduino. We have verified all USART register configurations are correct at the hardware level. A full GPIO scan of every MCU pin (PA0–PG15) shows zero toggling signal from the sensor. We suspect a board-level routing issue (solder bridges) but need ST guidance.
Approach History
Phase 1: Custom STM32H7 Firmware
We wrote custom firmware using STM32H7 HAL to communicate with the sensor at 57600 baud via USART1 on PB6(TX)/PB7(RX). Console output via USART3 PD8/PD9 (ST-Link VCP) works correctly.
Phase 2: Porting Vendor F1 Reference Code to H7
We also ported the sensor vendor's official STM32F1 sample code to STM32H7 HAL. This scans all standard baud rates (4800–921600) and attempts to detect the sensor. Same result — zero bytes received.
Phase 3: Tested Multiple Pin Configurations
- USART1 on PB6(TX)/PB7(RX) (AF7) — Arduino D1/D0 per UM2407 Table 21
- USART6 on PG14(TX)/PG9(RX) (AF7) — alternate D1/D0 routing on some MB1364 configs
Both configurations: zero received bytes at all baud rates. Both cable orientations tested.
Phase 4: Register-Level Verification
We dumped all relevant registers and confirmed they are 100% correct:
USART1->CR1 = 0x0000002D (UE=1, RE=1, TE=1, RXNEIE=1) USART1->BRR = 0x006D (correct for 921600 @ 100MHz PCLK2) USART1->ISR = 0x006000D0 (TEACK=1, REACK=1, TXE=1, TC=1, IDLE=1) GPIOB->MODER = 0xFFFFAEBD (PB6=AF mode, PB7=AF mode) GPIOB->AFR[0] = 0x77000000 (PB6=AF7, PB7=AF7 = USART1)
Phase 5: GPIO Pin Activity Sampling (PB7)
We sampled PB7 (USART1 RX) 500,000 times in a tight loop:
PB7 sample: highs=500000 lows=0
Pin is permanently HIGH (idle). No UART start bits detected.
Phase 6: Full MCU GPIO Scan (All 112 Pins)
We scanned every GPIO pin on the entire MCU (PA0 through PG15), configuring each as input with internal pull-up, and sampling 100,000 times:
FULL MCU SCAN (PA0-PG15, 112 pins total): *** PA1: H=50774 L=49226 SIGNAL *** <- Ethernet PHY RMII_REF_CLK (expected) Scan complete. NO other toggling pins found on entire MCU.
What We Have Confirmed
Item Status
| Sensor works on Arduino (same unit, same baud, same wires) | Confirmed |
| Console UART (USART3 PD8/PD9 VCP) works correctly | Confirmed |
| USART1 registers 100% correct (CR1, BRR, ISR) | Verified via dump |
| GPIO MODER and AFR correct for PB6/PB7 AF7 | Verified via dump |
| NVIC interrupt enabled for USART1 | Verified |
| PB7 shows no signal activity (500K samples) | Confirmed stuck HIGH |
| Full MCU GPIO scan — no sensor signal on any pin | Confirmed |
| Tried USART1 (PB6/PB7) and USART6 (PG14/PG9) | Both zero bytes |
| All 9 baud rates tested (4800-921600) | All zero bytes |
| Both TX/RX cable orientations tested | Both tried |
| Clock config: HSE bypass 8MHz, SYSCLK 400MHz, PCLK2 100MHz | Confirmed good clocks |
Hardware Setup
- Board: Nucleo-H753ZI (MB1364, ST-LINK V3, rev B)
- Sensor UART target: USART1 on PB6(TX)/PB7(RX) = Arduino D1/D0 on CN10
- Console UART: USART3 on PD8(TX)/PD9(RX) = VCP (working)
- External device: WitMotion HWT9053 IMU (3.3V TTL UART, confirmed working on Arduino)
- Connection: Direct wire — sensor TX to CN10 D0: pin 16 (PB7), sensor RX to CN10 D1: pin 14 (PB6), GND to GND
Questions for ST
- Conflicts: Are there any known conflicts with PB6/PB7 on MB1364 (e.g., Ethernet, USB, ST-Link debug) that could prevent USART1 from functioning even with correct solder bridge configuration?
- GPIO scan interpretation: Our full-MCU GPIO scan detected no signal on any of the 112 scanned pins (only PA1 Ethernet PHY clock). Does this conclusively indicate the external signal is not reaching the MCU die, or could there be a scenario where the signal reaches the pin but is not visible to a GPIO input read?
- Alternative test method: Is there a recommended minimal hardware test to confirm that the CN10 D0/D1 header pins are electrically connected to PB6/PB7? (e.g., external pulldown on D0, read PB7 as GPIO input)
- Known issues: Are there any known errata or board-level issues with USART1 on PB6/PB7 for the Nucleo-H753ZI MB1364?
- References: Are there any STM32H7 UART bring-up examples, internal app-note snippets, or known-good MB1364 code/config templates that support can share for external sensor links?