Question
NPU and CPU power consuption measurment
Hi
For some of my project, I need to measure the power consumption of the STM32N6570-DK while running a model on the CPU only versus an NPU + CPU accelerated workload.
I am following the guide
Based on these documents, I plan to measure the current via CN2 pins 3 and 4 while powering the board through CN6 (USB-C).
My Question:
Does measuring current at this point (CN2 pins 3 & 4) isolate the consumption of the NPU and CPU (VDDCore)? Specifically, I want to know if this measurement will include the power draw from the camera module and LCD display if they are active in the same project.
Does measuring current at this point (CN2 pins 3 & 4) isolate the consumption of the NPU and CPU (VDDCore)? Specifically, I want to know if this measurement will include the power draw from the camera module and LCD display if they are active in the same project.
Any guidance on isolating the core MCU power from the peripheral power would be greatly appreciated.