Skip to main content
Karl Yamashita
Principal
October 1, 2024
Solved

Nucleo-C031C6 duplicate net name on Morpho connector

  • October 1, 2024
  • 3 replies
  • 1818 views

 

I believe that the net name on CN7-4 should be PD3. 

Nucleo-C031_doubleNetname.jpg

Best answer by STTwo-32

Hello @Karl Yamashita @Andrew Neil 

After checking with our HW team, I can confirm that both connectors CN7-3 and CN7-4 are mapped to the same pin of the MCU (PD2).

Best Regards.

STTwo-32

3 replies

STTwo-32
Technical Moderator
October 1, 2024

Hello @Karl Yamashita 

Thank you for this contribution. I'm checking internally and i will be back to you ASAP.

Best Regards.

STTwo-32

Andrew Neil
Super User
October 1, 2024

Fig 7 in UM2953 is the same:

AndrewNeil_1-1727801087393.png

 

PS:

PD3 is on CN10.1 both in schematic and in UM2953 Fig 7

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
STTwo-32
STTwo-32Best answer
Technical Moderator
October 1, 2024

Hello @Karl Yamashita @Andrew Neil 

After checking with our HW team, I can confirm that both connectors CN7-3 and CN7-4 are mapped to the same pin of the MCU (PD2).

Best Regards.

STTwo-32

Karl Yamashita
Principal
October 1, 2024

As @Andrew Neil, PD3 is on CN10, which i missed.

Though it doesn't make sense to have PD3 by itself when it could have been grouped with the other 3 PDx pins. Unless there is a reason to have PD3 on CN10?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source