Skip to main content
Associate II
June 10, 2024
Question

Nucleo H723ZG docking options

  • June 10, 2024
  • 2 replies
  • 1052 views

Hello,

I want to use the Nucleo H723ZG for a project with analog & digital lines and can't find the article number of the headers CN7, CN8, CN9, CN10. Is there a specific cable/contact type I can use to plug in the black header body? Or are the headers pins at the bottom of the board meant to dock on some connector? Are there recommended docker boards like from Seeed Studio?

Many thanks 

2 replies

mƎALLEm
Technical Moderator
June 10, 2024

Hello,

Not pretty clear  ..

The CNx pinout description are provided in UM2407 Table 18 to Table 21.

You can develop your own board that fit these connectors and plug the Nucleo to it.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
Andrew Neil
Super User
June 10, 2024

You mean what ST call the "Zio" connectors:

AndrewNeil_0-1718011951219.png

As it says there, these will mate with standard ARDUINO® Uno V3 shields - so they are just 0.1" pitch headers, on the Arduino layout.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.