NUCLEO-H755ZI: ST-LINK detected but “No STM32 target found / Unable to get core ID”
Hello STM32 Community,
I am a newbie and facing an issue with my NUCLEO-STM32H755ZI board.
I am unable to connect to the STM32H755 target using STM32CubeProgrammer, even though the ST-LINK appears to be working correctly,
Hardware
Board: NUCLEO-STM32H755ZI
Debugger: On-board ST-LINK
USB connection: CN1 (USB-A to Micro-B).
Software
STM32CubeProgrammer: v2.21.0
OS: Windows
Connection mode: ST-LINK / SWD
Observed Behavior
ST-LINK is detected correctly by Windows
ST-LINK Virtual COM Port is visible in Device Manager
Target voltage ~3.27 V is shown in Cube programmer.
Green power LED (LD3) is
- Red ST-LINK LED is blinking
- Error: No STM32 target found!
Unable to get core ID
If your product embeds Debug Authentication,
please perform a discovery using Debug Authentication