Skip to main content
Associate
September 13, 2025
Question

Nucleo-H7S3L8 MIPI20 to J-Link

  • September 13, 2025
  • 2 replies
  • 1221 views

Hello Everyone,

 

I have the Nucleo-H7S3L8 as my first STM32 board.

 

I want to connect it to a Segger J-Link Pro for JTAG. In the official documentation (https://www.st.com/resource/en/user_manual/um3276-stm32h7rx7sx-nucleo144-board-mb1737-stmicroelectronics.pdf), the board supports JTAG debugging through the MIPI20 connector CN1 (7.3.3 on page 14). For a more detailed view, see Figure 4 on Page 10.

 

I am looking for a way to connect MIPI20 (male pins) to the ARM-20 pins on the J-Link. Is there a way to connect the two?

2 replies

KDJEM.1
Technical Moderator
October 8, 2025

Hello @C24 and welcome to the community;

 

To connect the MIPI20 male pins on the Nucleo-H7S3L8 board to the ARM-20 pins on a Segger J-Link for JTAG debugging, you can use specific adapters or cables. To choice the adequate cable you need to refer to the Segger J-Link documentation for the ARM-20 pinout.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
October 8, 2025

@C24 wrote:

I am looking for a way to connect MIPI20 (male pins) to the ARM-20 pins on the J-Link. Is there a way to connect the two?


It's just a pin header - you can check details in the BoM.

You just need to wire the necessary pins from that header to the corresponding pins on the J-Link.

Nothing special required.

You should also find that the necessary debug pins (SWDIO,SWCLK,NRST) are available on the "Morpho headers" - so you could wire to them...

 

You could ask Segger if they have a suitable adaptor...

https://www.segger.com/support/technical-support/

https://forum.segger.com/board/4-j-link-flasher-related/

 

PS:

It looks to be compatible with the Standard ARM Cortex Debug+ETM pinout:

AndrewNeil_0-1759913782583.png

https://documentation-service.arm.com/static/5fce6c49e167456a35b36af1#page=2

See also: 

https://developer.arm.com/documentation/101416/0100/Introduction/CoreSight-Technology/Connectors

 

PPS:

See also: https://www.samtec.com/standards/jtag

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.