Skip to main content
Associate II
November 7, 2025
Question

port the STEVAL-STWINBX1 firmware to my custom hardware

  • November 7, 2025
  • 1 reply
  • 265 views

Post edited by ST moderator to be inline with the community rules for the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code.

Hi,

I’m now trying to port the STEVAL-STWINBX1 firmware to my custom hardware whose MCU is STM32U575VGT6. 
I started by porting the data logging application:

fp-sns-datalog2\STM32CubeFunctionPack_DATALOG2_V3.1.0\Projects\STM32U585AI-STWIN.box\Applications\DATALOG2
During execution the following code gets stuck,and eventually returns HAL_ERROR.

/* Wait for calibration completion */
while (LL_ADC_IsCalibrationOnGoing(hadc->Instance) != 0UL)
{
wait_loop_index++;
if (wait_loop_index >= ADC_CALIBRATION_TIMEOUT)
{
/* Update ADC state machine to error */
ADC_STATE_CLR_SET(hadc->State, HAL_ADC_STATE_BUSY_INTERNAL, HAL_ADC_STATE_ERROR_INTERNAL);

__HAL_UNLOCK(hadc);

return HAL_ERROR;
}

I’ve verified that the hardware is fine with my own test program (DAC generates a sine wave, ADC samples it, and I print the data over USART).  I’m not sure what’s wrong—could you give me some suggestions?

zefang

1 reply

SimonePradolini
Technical Moderator
November 14, 2025

Hello @dzf 

I've just downloaded your example and started debugging. I'll come back to you in a few days.

 

Best regards,

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.