Skip to main content
Associate
October 26, 2025
Solved

Putty not receiving Data from NUCLEO-F303ZE

  • October 26, 2025
  • 3 replies
  • 701 views

Title edited to be clear that this is on a NUCLEO-F303ZE board.


Hello all.

I'm trying to write a simple message via UART to Putty using stm32f303ze microcontroller. I'm using USART2, via ST-link. All the configurations have been confirmed (baud rate, COM port, bits, etc.) And they are right. I even tried using the STM32 Cube IDE Terminal with no luck. Now I'm not sure if the problem is the UART I'm using, or I'm doing something wrong in the code.

Also I'm not sure about the UART that support VCP in STM32F303ZE microcontrollers. However I tried all the USART, and the were no response in the Terminals.

 

Below is the simple message I'm trying to send and the full code.

/* USER CODE BEGIN Header */

/**

 ******************************************************************************

 * @file : main.c

 * @brief : Main program body

 ******************************************************************************

 * @attention

 *

 * Copyright (c) 2025 STMicroelectronics.

 * All rights reserved.

 *

 * This software is licensed under terms that can be found in the LICENSE file

 * in the root directory of this software component.

 * If no LICENSE file comes with this software, it is provided AS-IS.

 *

 ******************************************************************************

 */

/* USER CODE END Header */

/* Includes ------------------------------------------------------------------*/

#include "main.h"



/* Private includes ----------------------------------------------------------*/

/* USER CODE BEGIN Includes */

#include <string.h>





/* USER CODE END Includes */



/* Private typedef -----------------------------------------------------------*/

/* USER CODE BEGIN PTD */



/* USER CODE END PTD */



/* Private define ------------------------------------------------------------*/

/* USER CODE BEGIN PD */



/* USER CODE END PD */



/* Private macro -------------------------------------------------------------*/

/* USER CODE BEGIN PM */



/* USER CODE END PM */



/* Private variables ---------------------------------------------------------*/

UART_HandleTypeDef huart2;



/* USER CODE BEGIN PV */



/* USER CODE END PV */



/* Private function prototypes -----------------------------------------------*/

void SystemClock_Config(void);

static void MX_GPIO_Init(void);

static void MX_USART2_UART_Init(void);

/* USER CODE BEGIN PFP */



/* USER CODE END PFP */



/* Private user code ---------------------------------------------------------*/

/* USER CODE BEGIN 0 */







/* USER CODE END 0 */



/**

 * @brief The application entry point.

 * @retval int

 */

int main(void)

{



 /* USER CODE BEGIN 1 */



 /* USER CODE END 1 */



 /* MCU Configuration--------------------------------------------------------*/



 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

 HAL_Init();



 /* USER CODE BEGIN Init */



 /* USER CODE END Init */



 /* Configure the system clock */

 SystemClock_Config();



 /* USER CODE BEGIN SysInit */



 /* USER CODE END SysInit */



 /* Initialize all configured peripherals */

 MX_GPIO_Init();

 MX_USART2_UART_Init();

 /* USER CODE BEGIN 2 */





 /* USER CODE END 2 */



 /* Infinite loop */

 /* USER CODE BEGIN WHILE */

 while (1)

 {

 /* USER CODE END WHILE */



 /* USER CODE BEGIN 3 */

 char msg[] = "UART test OK\r\n";



 HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);

 HAL_Delay(1000);



 }

 /* USER CODE END 3 */

}



/**

 * @brief System Clock Configuration

 * @retval None

 */

void SystemClock_Config(void)

{

 RCC_OscInitTypeDef RCC_OscInitStruct = {0};

 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};



 /** Initializes the RCC Oscillators according to the specified parameters

 * in the RCC_OscInitTypeDef structure.

 */

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

 RCC_OscInitStruct.HSIState = RCC_HSI_ON;

 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;

 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;

 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

 {

 Error_Handler();

 }



 /** Initializes the CPU, AHB and APB buses clocks

 */

 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;

 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;



 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)

 {

 Error_Handler();

 }

 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART2;

 PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;

 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)

 {

 Error_Handler();

 }

}



/**

 * @brief USART2 Initialization Function

 * None

 * @retval None

 */

static void MX_USART2_UART_Init(void)

{



 /* USER CODE BEGIN USART2_Init 0 */



 /* USER CODE END USART2_Init 0 */



 /* USER CODE BEGIN USART2_Init 1 */



 /* USER CODE END USART2_Init 1 */

 huart2.Instance = USART2;

 huart2.Init.BaudRate = 115200;

 huart2.Init.WordLength = UART_WORDLENGTH_8B;

 huart2.Init.StopBits = UART_STOPBITS_1;

 huart2.Init.Parity = UART_PARITY_NONE;

 huart2.Init.Mode = UART_MODE_TX_RX;

 huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;

 huart2.Init.OverSampling = UART_OVERSAMPLING_16;

 huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;

 huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;

 if (HAL_UART_Init(&huart2) != HAL_OK)

 {

 Error_Handler();

 }

 /* USER CODE BEGIN USART2_Init 2 */



 /* USER CODE END USART2_Init 2 */



}



/**

 * @brief GPIO Initialization Function

 * None

 * @retval None

 */

static void MX_GPIO_Init(void)

{

 /* USER CODE BEGIN MX_GPIO_Init_1 */



 /* USER CODE END MX_GPIO_Init_1 */



 /* GPIO Ports Clock Enable */

 __HAL_RCC_GPIOA_CLK_ENABLE();



 /* USER CODE BEGIN MX_GPIO_Init_2 */



 /* USER CODE END MX_GPIO_Init_2 */

}



/* USER CODE BEGIN 4 */



/* USER CODE END 4 */



/**

 * @brief This function is executed in case of error occurrence.

 * @retval None

 */

void Error_Handler(void)

{

 /* USER CODE BEGIN Error_Handler_Debug */

 /* User can add his own implementation to report the HAL error return state */

 __disable_irq();

 while (1)

 {

 }

 /* USER CODE END Error_Handler_Debug */

}

#ifdef USE_FULL_ASSERT

/**

 * @brief Reports the name of the source file and the source line number

 * where the assert_param error has occurred.

 * file: pointer to the source file name

 * line: assert_param error line source number

 * @retval None

 */

void assert_failed(uint8_t *file, uint32_t line)

{

 /* USER CODE BEGIN 6 */

 /* User can add his own implementation to report the file name and line number,

 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */

 /* USER CODE END 6 */

}

#endif /* USE_FULL_ASSERT */

Post edited by ST moderator to be inline with the community rules for the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code.

 

Best answer by Athandile

Thank you so much, it’s working now.

I noticed that PB10 and PE15 were automatically configured by STM32CubeIDE when I enabled the USART during configuration. I saw in the datasheet that multiple pins are associated with each U(S)ART, but I’m struggling to understand how to determine which pins to use and when.

The IDE automatically assigns pins linked to a specific register, but I’d like to understand the logic or criteria behind this process. How am I suppose to know that USART is attached to PD8 and PD9 while the IDE enabled the other pins? I’ve attached some images from one datasheet for your reference.

Thank you once again for your guidance and support.Screenshot 2025-10-28 010332.pngScreenshot 2025-10-28 010230.png

3 replies

TDK
Super User
October 26, 2025

Is the the NUCLEO-F303RE board? Are you trying to use the ST-Link's VCP? The VCP is connected to USART3 over PD8/PD9 by default.

"If you feel a post has answered your question, please click ""Accept as Solution""."
AthandileAuthor
Associate
October 26, 2025

I'm using NUCLEO-F303ZE board. Yes I'm tryjng to use the ST-Link's VCP, and I did try to use USART 3 but it didn't work. 

TDK
Super User
October 27, 2025

Try again, and if you can't get it, post the code you are using along with the IOC file. The code you posted won't work as it uses USART2.

There are also working examples you can follow.

STM32CubeF3/Projects/STM32F303ZE-Nucleo/Examples/UART/UART_Printf at master · STMicroelectronics/STM32CubeF3

"If you feel a post has answered your question, please click ""Accept as Solution""."
AthandileAuthor
Associate
October 27, 2025

Still I'm not getting anything. Below is the code with the IOC file as requested.

Technical Moderator
October 27, 2025

Hello @Athandile 

The pins associated with UART3 VCP are PD8 and PD9. However, in your IOC file, you have configured PB10 and PE15 instead.

Saket_Om_0-1761557394237.png

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"
AthandileAuthor
Associate
October 27, 2025

Thank you so much, it’s working now.

I noticed that PB10 and PE15 were automatically configured by STM32CubeIDE when I enabled the USART during configuration. I saw in the datasheet that multiple pins are associated with each U(S)ART, but I’m struggling to understand how to determine which pins to use and when.

The IDE automatically assigns pins linked to a specific register, but I’d like to understand the logic or criteria behind this process. How am I suppose to know that USART is attached to PD8 and PD9 while the IDE enabled the other pins? I’ve attached some images from one datasheet for your reference.

Thank you once again for your guidance and support.

Screenshot 2025-10-28 010332.pngScreenshot 2025-10-28 010230.png

Andrew Neil
Super User
October 27, 2025

@Athandile wrote:

I'm not sure about the UART that support VCP in STM32F303ZE microcontrollers.


The UART itself doesn't have anything to do with VCP - it's just a UART.

The VCP is part of the ST-Link on the Nucleo board.

The Nucleo board provides the physical connection from the STM32F303ZE microcontroller to the VCP in the ST-Link:

AndrewNeil_0-1761576479875.png

Details of which UART and which pins are used:

AndrewNeil_1-1761576559762.png

https://www.st.com/resource/en/user_manual/um1974-stm32-nucleo144-boards-mb1137-stmicroelectronics.pdf#page=27

via: https://www.st.com/en/evaluation-tools/nucleo-f303ze.html#documentation

 

You can also check this in the board schematics - see the 'CAD Resources' tab on the board's Product Page:

https://www.st.com/en/evaluation-tools/nucleo-f303ze.html#cad-resources

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
AthandileAuthorBest answer
Associate
October 28, 2025

Thank you so much, it’s working now.

I noticed that PB10 and PE15 were automatically configured by STM32CubeIDE when I enabled the USART during configuration. I saw in the datasheet that multiple pins are associated with each U(S)ART, but I’m struggling to understand how to determine which pins to use and when.

The IDE automatically assigns pins linked to a specific register, but I’d like to understand the logic or criteria behind this process. How am I suppose to know that USART is attached to PD8 and PD9 while the IDE enabled the other pins? I’ve attached some images from one datasheet for your reference.

Thank you once again for your guidance and support.Screenshot 2025-10-28 010332.pngScreenshot 2025-10-28 010230.png