Skip to main content
Associate II
September 15, 2024
Question

Receiving ATE=0 on the Tera Term

  • September 15, 2024
  • 1 reply
  • 605 views

Hello,

I am implementing UART through the NUCLEO-L073RZ board, I have connected PA2 and PA3 pin of the board to the  FTDI and what I see on the Tera Term is ATE=0, not what I am sending, can anyone tell how to resolve the issue.

 

1 reply

Andrew Neil
Super User
September 15, 2024

You need to give some more details:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

 


@2001jolly wrote:

I have connected PA2 and PA3 pin of the board to the  FTDI


Note that, by default, those pins are connected to the ST-Link's VCP (Virtual COM Port) - so there's no need for a separate USB-to-UART adaptor:

AndrewNeil_0-1726394448240.png

 

If you do want to use a separate USB-to-UART adaptor, you will need to disconnect the pins from the ST-Link's VCP.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.