Skip to main content
Pavel A.
Super User
June 13, 2022
Solved

[RESOLVED] VCP on ST-LINK v3 mini

  • June 13, 2022
  • 4 replies
  • 5366 views

I cannot get the VCP function of ST-LINK v3 mini working.

Windows sees the com port and can open it

Connected TX output of UART to pin 14 of ST-LINK 3 mini, but nothing is received on the PC side.

Connected some other serial TTL-USB adapter (set to 3.3V), and it works properly.

However, the serial TTL-USB adapter has a ground connection and ST-LINK's VCP has common ground with other functions.

The debugger function works properly.

Is the TX level of VCP 3.3 or 5 V? Does the VCP function work for anyone?

Thanks,

-- pa

Best answer by Tesla DeLorean

Should be 3.3V

Make sure the RX/TX sense is not reversed. Stick a scope on the pins and send stream of data from PC​

4 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
June 13, 2022

Should be 3.3V

Make sure the RX/TX sense is not reversed. Stick a scope on the pins and send stream of data from PC​

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
Pavel A.
Pavel A.Author
Super User
June 13, 2022

It was a bad soldering. Some software folks are terrible solders (yes it's me). Thanks.

Tesla DeLorean
Guru
June 13, 2022

I'm an electronics guy, but my soldering skills aren't particularly good, but I have technicians with better skills/technique, better eyesight, and better equipment.. and a lot more practice.

Using high power irons (70-80W), with the right bits, right temperature, and right solder do improve the odds significantly.

I also don't like breadboards, and dupont wires, I much prefer wire-wrap and schmartboard jumper wires, type of thing with good metallic bonds, and can survive a trip around a conference table..

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
Paul1
Senior III
June 13, 2022

a) We use the STLINK com port all the time, very convenient with the 14pin MIPI connector.

b) Personally I wouldn't call that VCP as it can be easily confused with STM32 VCP support.

  • STLINK provides a USB COM port that can connect to UART pins on the STM32
  • STM32 VCP is a method of simulating UART through the STM's USB using only the D+/D- pins, and loading appropriate code in the STM32. We've been using this with USB-C connectors on our boards and it provides a nice robust non-orientation restricting connection which is real nice when the boards are in hard to reach places using easily available cables.

Paul

Associate II
March 1, 2025

This took  me a while to find how *** is the RX, TX on ST Link! how on earth they did this? 

RX which is receive pin is OUTPUT!, and TX is INPUT! this is most *** think I have ever seen in my life. such a waste of time ...

drafshin_0-1740845241297.png

 

Visitor II
November 9, 2025

try to connect TX with TX, RX with RX, STLINK V3 MINIE is not the same as other STLINK i have used.