Skip to main content
Associate II
August 8, 2025
Solved

[SOLVED] NUCLEO-C071RB Mass Storage not working. NOD_C071RB doesn't show up in Linux (Ubuntu 24.04)

  • August 8, 2025
  • 1 reply
  • 509 views

Hi!

TLDR; Mass Storage on STLINK on NUCLEO-C071RB isn't enabled by default. You need to use STLinkUpgrade to change Type to STM32 Debug+Mass Storage+VCP

I've got a new NUCLEO-C071RB for test purpose, to evaluate that it's ready to be programmed in my build environment. I quickly wanted to test it in the Arduino IDE with stm32duino board files. For simplicity I choose the upload method Mass Storage. I sat up the typical udev rules manually and added my user to dialout group, and restarted Ubuntu. After this, I still struggled to program the NUCLEO-C071RB board with Arduino IDE using the Mass Storage upload method.

That's when I had the idea to bring out a previous board I have laying around, NUCLEO-F401RE. Quickly after, this one was confirmed to work. At this moment i realized that NOD_F401RE was visible as an external storage on Ubuntu, while NOD_C071RB was not. Which confirmed that Mass Storage wasn't working on the NUCLEO-C071RB.

Update: I tried to see if there was any firmware updates for the STLINK. To keep the story short, STLinkUpgrade 3.16.8 requires additional permissions in Linux (Ubuntu 24.04) that I didn't look into. Ended up upgrading the STLINK firmware through Windows. Now I can program the NUCLEO-C071RB on my Ubuntu 24.04 computer with Arduino IDE utilizing the Mass Storage upload method.

(*) I read somewhere someone recommended using stws-link007 (Standalone STLinkUpgrade??). Which I see includes .sh scripts to setup udev rules. Possible that this script ensures access for firmware update for the STLINK with STLinkUpgrade software included in STM32CubeProgrammer.



Best answer by KDJEM.1

Hello @EngEmil and welcome to the community;

 

Thanks for sharing this case and the solution you found. ​

To make this post more visible and easier to find by others who may face the same issue, I mark my reply as the solution. 



@EngEmil wrote:


Update: I tried to see if there was any firmware updates for the STLINK. To keep the story short, STLinkUpgrade 3.16.8 requires additional permissions in Linux (Ubuntu 24.04) that I didn't look into. Ended up upgrading the STLINK firmware through Windows. Now I can program the NUCLEO-C071RB on my Ubuntu 24.04 computer with Arduino IDE utilizing the Mass Storage upload method.




Regards,

Kaouthar

1 reply

KDJEM.1
KDJEM.1Best answer
Technical Moderator
August 20, 2025

Hello @EngEmil and welcome to the community;

 

Thanks for sharing this case and the solution you found. ​

To make this post more visible and easier to find by others who may face the same issue, I mark my reply as the solution. 



@EngEmil wrote:


Update: I tried to see if there was any firmware updates for the STLINK. To keep the story short, STLinkUpgrade 3.16.8 requires additional permissions in Linux (Ubuntu 24.04) that I didn't look into. Ended up upgrading the STLINK firmware through Windows. Now I can program the NUCLEO-C071RB on my Ubuntu 24.04 computer with Arduino IDE utilizing the Mass Storage upload method.




Regards,

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.