Skip to main content
Associate
August 17, 2025
Solved

ST Link V3 for NUCLEO-H755ZI-Q

  • August 17, 2025
  • 1 reply
  • 596 views

Hello everyone, the STM32F723IEK6 chip on my H755ZI-Q development board is damaged. If I replace it with a brand new MCU, how can I restore the program

Best answer by AScha.3

Basically - yes/maybe. But firmware not same , it still will "know" its a st-link V3. And maybe says "error"....

afaik nobody did this .

ed: here he did it:

https://dalaotech.com/2021/08/26/1107/

(maybe, use translate...)

And big risk, if its not working , you just damaged board and st-link.

(de- and re-solder an BGA , you can do this with good experience on BGA rework?)

So better just buy an st-link miniE , has the 14pin ->

AScha3_0-1755420571192.png

AScha3_3-1755421205419.png

 

 

 

 

 

and your board has the 20pin ->

AScha3_1-1755420619557.png

So it should work with the cable in the "right" position : vdd , swd,...reset , matching the position on the cable connector vcc, swd...reset.

And maybe remove the dead F723 , if it heats up or is shorted.

btw

What you did , to be sure, the F723 is dead ?

 

1 reply

AScha.3
Super User
August 17, 2025

Hi,

you cannot.

Because STM keeps the st-link firmware secret, you only can buy a st-link V3 (miniE or mods , are not much more expensive than buying a F723 cpu).

"If you feel a post has answered your question, please click ""Accept as Solution""."
XSMSQAuthor
Associate
August 17, 2025

 Bro,Can I purchase ST Link V3 and transplant the chip

AScha.3
AScha.3Best answer
Super User
August 17, 2025

Basically - yes/maybe. But firmware not same , it still will "know" its a st-link V3. And maybe says "error"....

afaik nobody did this .

ed: here he did it:

https://dalaotech.com/2021/08/26/1107/

(maybe, use translate...)

And big risk, if its not working , you just damaged board and st-link.

(de- and re-solder an BGA , you can do this with good experience on BGA rework?)

So better just buy an st-link miniE , has the 14pin ->

AScha3_0-1755420571192.png

AScha3_3-1755421205419.png

 

 

 

 

 

and your board has the 20pin ->

AScha3_1-1755420619557.png

So it should work with the cable in the "right" position : vdd , swd,...reset , matching the position on the cable connector vcc, swd...reset.

And maybe remove the dead F723 , if it heats up or is shorted.

btw

What you did , to be sure, the F723 is dead ?

 

"If you feel a post has answered your question, please click ""Accept as Solution""."