Skip to main content
KBloo.1
Visitor II
August 20, 2024
Question

STEVAL-IDB00BV2

  • August 20, 2024
  • 0 replies
  • 495 views

All:

I have the IDB00BV2 and am using the Keil Uvision_5 tool with the compiler back leveled to version V5. I'm using this board to test software to be run on the BlueMRG-2 running on my product. I have the ST BlueNRG-1_2 DB32.3 Project software installed for the KEIL MDK.  I also have the STLINK V/2 connected to the board for programming and debug purposes

I have the following questions:

The board is supposed to come preloaded with running software that will on power up connect to a remote Bluetooth device such as an Iphone.  This does not appear to be working as I have multiple Blue tooth devices that do not see the board advertising.

Second- The IDB00BV2 does not show up as any of the boards in the KEIL packs.  Which Board should I select as the running board?

Third - Which processor should I use for the MDK? Right now I have selected the STM32F030C6Tx is that OK?

Appreciate any help or insight that can be offered.

Regards

KEn