Skip to main content
Visitor II
June 21, 2024
Question

STM32 Nucleo support for 1.8V

  • June 21, 2024
  • 1 reply
  • 644 views

Hi

I'm using the STM32H755ZI board which has the option for 1.8V DVDD (using JP5).

Does switching DVDD to 1.8V from 3.3V limit the functionality of the board in any way ?

Are the interfaces (CAN, I2C, SPI, UART etc) still functional at 1.8V ? 

Thanks in advance for any help

1 reply

Uwe Bonnes
Chief
June 22, 2024

Have a loo at the datasheet

5.3
Operating conditions
5.3.1
General operating conditions
E,g,USB needs 3 V minumum