Skip to main content
Associate
December 1, 2024
Solved

STM32F072B-DISCO and MEMS module (I3G4250D vs L3GD20)

  • December 1, 2024
  • 2 replies
  • 929 views

Hi ST,

Newbie question with regards to finding the right documentation.

I went through previous threads trying to find an answer to this but I have not come across anything.

I have an older iteration of the STM32F072B-DISCO board (as I've discovered!). I was able to use the STM32CubeF0 Samples/Demonstration/Example files that still expects L3GD20 and it worked out fine, however I realized the discrepancy in documentation because the WHO_AM_I identifier of the MEMS module was different on the board vs. the documentation of the datasheet. All of the new materials points to it using I3G4250D MEMS module, but I saw no mention of the module being changed in the Release/Change Notes anywhere.

I was only able to find the schematic diagram of the board that has the L3GD20 module on it, and no other documentation:

I3G4250D - https://www.st.com/resource/en/schematic_pack/mb1076-f072b-d02_schematic.pdf

L3GD20 - https://www.st.com/resource/en/schematic_pack/mb1076-f072b-c01_schematic.pdf

Would you be able to guide me as to how I can find the rest of the documentation for the iteration of the board I have? Not sure what else has changed and I'd rather not do something to destroy the board in the process.

Thank you!

Best answer by KDJEM.1

Hello @JS5,

Compared to the bill of materials, version D02 vs. C01:

- C9, C10 moved from 20 pF to 33 pF (foot capacitors of 8MHz STLINK XTAL)

- Added new C34 470 nF (due to MEMS change)

- Added new R45 10K (due to MEMS change)

- U3 changed from L3GD20TR to I3G4250D 

- U4 changed from STM32F052RBT6 to STM32F072RBT6

I reported this issue internally to add this information to UM1690.

Internal ticket number: 198933 (This is an internal tracking number and is not accessible or usable by customers).

 

Thank you for your contribution to the community.

Kaouthar

2 replies

KDJEM.1
Technical Moderator
December 18, 2024

Hello @JS5;

 

I reported this issue internally.

I will come back to you with more details as soon as possible.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
KDJEM.1
KDJEM.1Best answer
Technical Moderator
December 18, 2024

Hello @JS5,

Compared to the bill of materials, version D02 vs. C01:

- C9, C10 moved from 20 pF to 33 pF (foot capacitors of 8MHz STLINK XTAL)

- Added new C34 470 nF (due to MEMS change)

- Added new R45 10K (due to MEMS change)

- U3 changed from L3GD20TR to I3G4250D 

- U4 changed from STM32F052RBT6 to STM32F072RBT6

I reported this issue internally to add this information to UM1690.

Internal ticket number: 198933 (This is an internal tracking number and is not accessible or usable by customers).

 

Thank you for your contribution to the community.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.