Skip to main content
Franksterb92
Senior
February 1, 2025
Solved

STM32F429I-DISC1 BSP Question

  • February 1, 2025
  • 1 reply
  • 493 views

im looking in the bsp folder for the stm32f429i-disc in the stm32cube_fw_f4 folder and i see a file stm32f429i-discovery_eeprom.c why is this here as i dont believe there is a eeprom on this board 

Best answer by TDK

All of the ST source files are well commented. Here it what the file says it does:

 * @file stm32f429i_discovery_eeprom.c
 * @author MCD Application Team
 * @brief This file provides a set of functions needed to manage an I2C M24LR64
 * EEPROM memory.
 * To be able to use this driver, the switch EE_M24LR64 must be defined
 * in your toolchain compiler preprocessor
 *
 * ===================================================================
 * Notes:
 * - This driver is intended for STM32F4xx families devices only.
 * - The I2C EEPROM memory (M24LR64) is available on separate daughter
 * board ANT7-M24LR-A, which is not provided with the STM32F429I
 * DISCOVERY board.
 * To use this driver you have to connect the ANT7-M24LR-A to CN3
 * connector of STM32F429I DISCOVERY board.
 * ===================================================================

 

1 reply

TDK
TDKBest answer
Super User
February 1, 2025

All of the ST source files are well commented. Here it what the file says it does:

 * @file stm32f429i_discovery_eeprom.c
 * @author MCD Application Team
 * @brief This file provides a set of functions needed to manage an I2C M24LR64
 * EEPROM memory.
 * To be able to use this driver, the switch EE_M24LR64 must be defined
 * in your toolchain compiler preprocessor
 *
 * ===================================================================
 * Notes:
 * - This driver is intended for STM32F4xx families devices only.
 * - The I2C EEPROM memory (M24LR64) is available on separate daughter
 * board ANT7-M24LR-A, which is not provided with the STM32F429I
 * DISCOVERY board.
 * To use this driver you have to connect the ANT7-M24LR-A to CN3
 * connector of STM32F429I DISCOVERY board.
 * ===================================================================

 

"If you feel a post has answered your question, please click ""Accept as Solution""."