Skip to main content
Associate II
January 8, 2025
Question

STM32F469i-DISCO USB OTG-FS communication

  • January 8, 2025
  • 1 reply
  • 570 views

Greetings, we are using a STM32F469i-DISCO development board for one of our projects. We are unable to establish Host USB OTG FS communication. The USB shows that it is idle state so we are not able to transmit or receive any communication. We want to establish a Host USB OTG FS communication from the CN13 connector on this board to a device supporting USB via a Usb mini-b connector. We are trying to physically connect these 2 ports via a 'USB micro-b' - 'USB type A female adapter' - 'USB type A female adapter' - 'USB mini b'. The libraries that we use are the ones provided by STMicroelectronics. We are also not aware of how to ensure the host device is working, What can be the issue, we need to resolve this as soon as possible. Thank you

 

Regards,

Ashutosh

1 reply

Technical Moderator
April 3, 2025
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL