Skip to main content
Associate
March 24, 2025
Question

STM32F747XIH6 ST-Link Connection Issue – Unable to Flash Code

  • March 24, 2025
  • 2 replies
  • 1021 views

Hello, I have designed a circuit using the STM32F747XIH6, but I am unable to connect and flash the code using ST-Link. I have checked all the connections, and the NRST pin has a pull-up resistor and measures 3.3V. The 25MHz clock signal appears correct on the oscilloscope. The power circuit is designed in SMPS mode as per the datasheet, and the VFB_SMPS pin measures 1.2V. The VCORE1, VCORE2, and VCORE3 pins each have a 2.2µF capacitor and measure 1.0V. Despite these confirmations, I am still unable to connect via ST-Link and flash the code. Could there be any overlooked issue causing this?

2 replies

Peter BENSCH
Technical Moderator
March 25, 2025

Welcome @merbekta, to the community!

Please upload a legible photo of your ST-LINK (front and back).

Regards
/Peter

merbektaAuthor
Associate
March 25, 2025

Thank you for your response. I'm happy to be among you.. I tried to flash the program using both ST-Link V2 Mini and ST-LINK/V2, but I was unsuccessful. Both ST-Links were tested on other boards and are working properly.

WhatsApp Image 2025-03-25 at 1.51.30 PM.jpegWhatsApp Image 2025-03-25 at 1.52.58 PM.jpegWhatsApp Image 2025-03-25 at 1.52.20 PM.jpegWhatsApp Image 2025-03-25 at 1.51.31 PM.jpeg

Peter BENSCH
Technical Moderator
March 25, 2025

Unfortunately, I have to inform you that both ST-LINK/V2 are clones, i.e. equipped with fake STM32F103 and stolen firmware. However, software of STMicroelectronics can only support original hardware. Ok, the hardware costs a few bucks, but the very extensive software including all libraries is completely free to use.

Regards
/Peter

merbektaAuthor
Associate
March 25, 2025

I didn't know this. I will immediately acquire an original product. I assume you think the issue might be related to this hardware. After conducting my tests with the original product, I will write to you again. Thank you for your help.

Amel NASRI
Technical Moderator
March 26, 2025

Hi @merbekta ,

To help you acquire an original product, please refer to this article: How to recognize a genuine ST-LINK/V2 versus a cloned one

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.