Skip to main content
Associate II
February 8, 2024
Question

STM32H573-DK freeRTOS LWIP DHCP

  • February 8, 2024
  • 3 replies
  • 2110 views

Hi all.

Am working with the STM32H573-DK, trying to get the ethernet connection working with FreeRTOS & LWIP over DHCP.

I can see with Wireshark that it's sending the DHCP discover out ok & the DHCP server is responding with an offer but the code seems to miss that packet.

I know the code is receiving some ARP packets from the DHCP server.

I know that the hardware works ok if I use the ThreadX example (but I need a FreeRTOS environment).

My best guess so far is the DK is not receiving UDP packets? (Which is the format of the DHCP Offer)

Anyone else experienced similar with this DK?

 

3 replies

Visitor II
February 8, 2024

Check if there are any issues with buffer management in LWIP. Insufficient buffer space or incorrect buffer handling can lead to dropped packets.

pywtkAuthor
Associate II
February 8, 2024

Buffer structure-wise I've used the STM32H7 FreeRTOS & LWIP example as the basis for my H5 work. Are there any known "gotchas" with that Example?

Does that Example catch Buffer errors?

Haven't seen any serial debug or error_handler loops that'd suggest the proposed error has been detected.

 

ST Employee
February 12, 2024

Hello @pywtk ,

You can base your implementation on the working example (without FreeRTOS) and compare the configuration done on the STM32H5 with the one you are trying this can be a quick way to get it working .

Answering your question "Does that Example catch Buffer errors?"

The STM32H7 FreeRTOS & LWIP  does not catch buffer errors as it is a basic point to get started with your own software development .

BR

 

Visitor II
May 19, 2025

I know, your Question was a longer time ago, but were you succesful?
If yes, would you be able to share your code/experiences?

I am trying right now too, to use LwIP with FreeRTOS, and the DHCP part in the beginning seems to work fine, but as soon as I get to the Combination where the LwIP stuff has to work with FreeRTOS nothing seems to work as it should....

Thanks

Best
F.L