Skip to main content
Associate III
June 6, 2024
Solved

STM32H755 emmc compatibility - IS22TF08G-JCLA2

  • June 6, 2024
  • 2 replies
  • 1080 views

Hello,

In the RM0399 58.1 it is mentioned that EMMC is supported up to Version 4.51. I want to use the part  IS22TF08G-JCLA2 which supports a number of emmc interfaces up to 5.1 are these parts compatible? 

Best answer by KDJEM.1

Hello @sarun ,

The HS200 mode supported in IS22TF08G is compatible with STM32H755.

KDJEM1_1-1718103452213.png

 

KDJEM1_0-1718103370314.png

Thank you.

Kaouthar

2 replies

KDJEM.1
KDJEM.1Best answer
Technical Moderator
June 11, 2024

Hello @sarun ,

The HS200 mode supported in IS22TF08G is compatible with STM32H755.

KDJEM1_1-1718103452213.png

 

KDJEM1_0-1718103370314.png

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
sarunAuthor
Associate III
June 11, 2024

Thank you @KDJEM.1  for confirmation