Skip to main content
Associate II
November 13, 2024
Solved

stm32h755 power review

  • November 13, 2024
  • 3 replies
  • 3218 views

Hi,

I am designing a board based on STM32h755zit6 MCU and it's the first time for me working on this MCU, I am trying to simplify the design as possible to avoid any problem in the development, since we are short in time.
I found out that there is a firmware configuration for the power, is there a default configuration so I can make the hardware based on it? right now I made this schematic based on the Nucleo board, but I want to make sure that it's right configuration, Also I have the ST-link 2 is it possible to use it for programming? 

thanks 

Basel 

baselimadt_0-1731505805185.png

 

Best answer by mƎALLEm

Again please review the AN4938 "Getting started with STM32H74xI/G and STM32H75xI/G MCU hardware" development:

SofLit_0-1731590016221.png

And reference design schematics:

SofLit_1-1731590140921.png

 

 

3 replies

mƎALLEm
Technical Moderator
November 13, 2024

Hello @baselimadt and welcome to the community,

Better to remove the grid from the background in your schematics for more visibility.

Thanks.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
Associate II
November 13, 2024

here is a picture without it 

baselimadt_0-1731512095636.png

 

Andrew Neil
Super User
November 13, 2024
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Visitor II
November 13, 2024

Shouldn't there be a pull-up resistor (typically 10 kΩ)  connected to the NRST pin?

mƎALLEm
Technical Moderator
November 13, 2024

No need for external pull-up resistor on NRST pin. There is one internal:

SofLit_0-1731508901755.png

 

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
Sco
ST Employee
November 14, 2024

From hardware point of view:

1. STLINK V2 VS STLINK V3, the main point is speed. 

2. I reminder you that pin17(VFBSMPS) is an input pin, not a power pin.

3. Normally, if it's a first design your side, to reserve some 0R would be better, easier to debug.