Skip to main content
Associate III
January 29, 2025
Solved

stm32h7b3i-dk : Is it possible to use touchgfx / LCD and analog audio input at the same time

  • January 29, 2025
  • 1 reply
  • 565 views

Hi,

I am not able to understand the pin mapping in stm32h7b3i-dk (default pin mapping). I wont be using stmod+ but I need to use analog audio input (3.5mm Audio jack in) . By using the default set of pin mapping is it possible to use TouchGFX monitor and analog audio input without pin conflict? I tried to check this out myself my I am slightly confused about this.

 

Thank you in advance!

Best answer by mƎALLEm

Hello,

The only ressource I can see from the board's schematic is the I2C4:

The Audio codec:

SofLit_1-1738187767546.png

The LCD:

SofLit_2-1738187823669.png

But since it's an I2C I don't think it's an issue. The mux is managed by I2C device address.

 

1 reply

mƎALLEm
mƎALLEmBest answer
Technical Moderator
January 29, 2025

Hello,

The only ressource I can see from the board's schematic is the I2C4:

The Audio codec:

SofLit_1-1738187767546.png

The LCD:

SofLit_2-1738187823669.png

But since it's an I2C I don't think it's an issue. The mux is managed by I2C device address.

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
AmrithHNAuthor
Associate III
January 30, 2025

Thank You so much @mƎALLEm . I had my doubts cleared now, really appreciate your support .

 

Have a nice day!