Skip to main content
Associate II
September 22, 2025
Solved

STWIN.box Wi-Fi Module FW Upgrade - EMW3080

  • September 22, 2025
  • 5 replies
  • 1479 views

Hello 

I tried to upgrade the STWIN.box Wi-Fi Module with the instructions provided in the  STM32CubeFunctionPack_DATALOG2_V3.1.0. 

i tried dragging the HEX file to tera term with the following settings attached in the images below. i was not able to successfully upgrade the wifi module.
i am using the stlink-v3minie with the board
i really appreciate the help of community members

kind regards

Jose John

Best answer by josejohn

Thank you @SimonePradolini for your reply.
i was successfully able to flash the device.

Screenshot 2025-10-03 155926.png
kind regards
Jose John

5 replies

SimonePradolini
Technical Moderator
September 24, 2025

Hello @josejohn 

From the screenshots you shared, it seems you're not selecting the right COM port.

Once you link STWIN.box + STLINK to the PC, you should select the STLINK COM port named STMicroelectronics STLink Virtual COM Port, as in the above figure: 

SimonePradolini_0-1758728389354.png

Can you double check, use the proper port, and confirm me that the Wi-Fi firmware update procedure goes properly?

 

Best regards,

Simone

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
josejohnAuthor
Associate II
September 29, 2025

Thank you so much @SimonePradolini for looking into this matter. i still wasn't able to solve the problem. i have uploaded pictures of the same, the settings which are in my PC. i tried dragging the hex file to TeraTerm.  It can be seen that file is being transferred at a very low speed. i tried doing it multiple times. but the transfer was never ending.

1.png

2.png

3.png

could you please look into this.

kind regards
Jose John

josejohnAuthor
Associate II
September 29, 2025

Apart from the above images attached these are the other images of the settings, as only 3 images are allowed to upload in a post.

4.png

5.png

SimonePradolini
Technical Moderator
September 30, 2025

Hello @josejohn 

The hex file is a binary you must flash onto the STWIN.box core system. To do so, you can:

  • flash the board by using STM32CubeProgrammer
    SimonePradolini_0-1759217793619.png
  • drag-and-drop the hex file to the STLINK via file explorer
    SimonePradolini_1-1759217981065.png

     

Once the new firmware is uploaded, then you'll see the expected output on the terminal console and then you can upgrade the Wi-Fi module.

The procedure related to Tera Term isn’t related to the flashing of the hex file. I'm sorry if the README file wasn’t clear. I'll upgrade it soon with some more specific guidelines.

 

Best regards,

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
josejohnAuthor
Associate II
October 2, 2025

Thank you @SimonePradolini  for your detailed reply. i tried flashing the HEX file with STM32 programmer and it says download was successful. but after that the device was not be able to connect to my phone app. the GREEN LED was was not blinking but it was in a on state..
In the second image you shared i can't find the device STLNIK_V3M under My PC to drag and drop. I'm using STLINK_V3minie.
should i try in a different PC?
Is there any way to troubleshoot this

kind regards
Jose John

Screenshot 2025-09-30 170030.png

Screenshot 2025-09-30 154907.png

SimonePradolini
Technical Moderator
October 3, 2025

Hello,

The STM32CubeProgrammer procedure is the same as doing drag and drop. From your screenshots, I got that you flashed properly the Wi-Fi utility firmware. You should have already opened Tera Term with the already-cited parameters. So, you must simply follow the instructions on the terminal. Once you flashed the board through STM32CubeProgrammer, did you get the expected output from the terminal? No phone app is mentioned nor here neither in the README, I'm not understanding what you are referring for. 

STLINK_V3M or STLINK-V3MINIE are similar products. Yours is more recent than mine, but the functionalities are the same. It works in the same way; no need to search for a different PC.

 

Best regards,

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
josejohnAuthorBest answer
Associate II
October 3, 2025

Thank you @SimonePradolini for your reply.
i was successfully able to flash the device.

Screenshot 2025-10-03 155926.png
kind regards
Jose John

SimonePradolini
Technical Moderator
October 17, 2025

Hello @islavv 

Excuse me, but I'm a bit confused. The goal of the script we're providing inside FP-SNS-DATALOG2 is to be used for STEVAL-STWINBX1 only. We tested and can guarantee compatibility with STWINBX1 only and with the firmware we’re publicly exposing.

I agree with you that the latest MXCHIP firmware we're providing isn’t so recent. I can push your request internally.

As responsible for the FP-SNS-DATALOG2 package, I can update the function pack as soon as an upgraded MXCHIP firmware is validated internally by ST.

 

Best regards,

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
SimonePradolini
Technical Moderator
October 20, 2025

Hello @islavv 

I checked internally with the team responsible for the X-WIFI-EMW3080B package. Version v1.1.0 is still up to date, even if 2 years old. The maintainer would address firmware blocking point only.

Furthermore, I can't find a newer Wi-Fi module firmware from MXCHIP.

In conclusion, the Wi-Fi procedure for STEVAL-STWINBX1 with FP-SNS-DATALOG2 is still valid and up to date.

If instead you’re addressing some specific blocking point on the Wi-Fi upgrade procedure for other STEVAL or DISCOVERY boards, I suggest you open a new and separate thread.

 

Best regards,

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.