SWV works with NUCLEO-144 USB ST-LINK but not with external ST-LINK/V2
Hi,
I’m using a NUCLEO-144 (STM32H563ZIT6) development board with only the board USB STLINK-V3EC port connected. TRACE and DEBUG are enabled with Serial Wire in the configuration file, and printf is routed through ITM:
int _write(int file, char *ptr, int len) {
for (int i = 0; i < len; i++) {
ITM_SendChar((*ptr++));
}
return len;
}
SWV is enabled in the debug configuration, the core clock is 250 MHz, and the SWV window (port 0) shows output correctly in STM32CubeIDE.

When I switch to an external ST-LINK/V2 and connect

NRST#15 / SWDIO#7 / SWCLK#9 / GND#20 / TARGET VCC#1 / VDD3.3 V#19, programming and debugging work, but the SWV window shows nothing in the STM32CubeIDE.
The reason for using ST-LINK/V2 for SWV debugging is that on our product’s onboard MCU, only VDD, NRST, SWDIO, SWCLK, and GND are exposed.
Could anyone explain why SWV output does not appear with ST-LINK/V2?
Thanks.