Skip to main content
Associate II
October 22, 2024
Question

VBAT Pin for RTC Power Supply on STM32F407G-DISC1 Board

  • October 22, 2024
  • 2 replies
  • 757 views

I would like to know if the STM32F407G-DISC1 development board has a dedicated VBAT pin for powering the internal RTC, allowing it to maintain time even when the board is not connected to power. If there is no VBAT pin on the development board, does the STM32F407 microcontroller itself have a VBAT pin that can be utilized when designing a custom board using the microcontroller?

 

2 replies

Andrew Neil
Super User
October 22, 2024
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
EZHON.1
ST Employee
October 23, 2024