Skip to main content
Associate III
March 17, 2025
Solved

WiFi on STM32L4 B-L475E-IOT01A ISM43362-M3G-L44

  • March 17, 2025
  • 4 replies
  • 1206 views

Hi, 

I am using the STM32L4 B-L475E-IOT01A board with Wi-Fi module Inventek system ISM43362-M3G-L44.

I have seen the example WiFi projects but they do not have the .ioc file. So my question is, is there any middleware available in STM32CubeMX which can help me implement WiFi connectivity via USART? 

The communication interface between the stm32 board and the WiFi module is SPI3 by default but the documentation says that use of USART3 is also possible, and USART3 is what I want to use.

So any easy ways to do that? Any available middleware in CubeMX? Or is any example project available online?

Thanks!

Best answer by Andrew Neil

@fa31 wrote:

I have seen the example WiFi projects but they do not have the .ioc file. !


Indeed - not all projects have .ioc files:

https://community.st.com/t5/stm32-mcus-products/some-example-projects-don-t-use-ioc-file/m-p/698338/highlight/true#M255312

 

On the Inventek ISM43362 WiFi module, and ST examples:

https://community.st.com/t5/stm32cubeide-mcus/interface-onboard-wifi-module-of-stm32bl475/m-p/784098/highlight/true#M35031

4 replies

Pavel A.
Super User
March 17, 2025
Andrew Neil
Andrew NeilBest answer
Super User
March 18, 2025

@fa31 wrote:

I have seen the example WiFi projects but they do not have the .ioc file. !


Indeed - not all projects have .ioc files:

https://community.st.com/t5/stm32-mcus-products/some-example-projects-don-t-use-ioc-file/m-p/698338/highlight/true#M255312

 

On the Inventek ISM43362 WiFi module, and ST examples:

https://community.st.com/t5/stm32cubeide-mcus/interface-onboard-wifi-module-of-stm32bl475/m-p/784098/highlight/true#M35031

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
fa31Author
Associate III
March 18, 2025

The https://github.com/nano256/ISM43362-M3G-L44-Driver repo that was mentioned in one of your links, worked for me.

Thanks!

If anyone wants to know how:

I copied the wifi.c and wifi.h files, commented out the "#include "helper_functions.h"" line from wifi.c file and modified my main.c. Then I stepped into the code and added "wifiRxBuffer" variable into watch and saw that it was getting response from the WiFi-module. 

CubeMX modifications: I matched the cubemx configurations of the project with mine. Enabled SPI3 with the same settings, added GPIOs with same labels. 

 

Associate II
June 17, 2025

Hi can you please tell me which pins did you use and what did you put in your main.c 
Thank you!

Andrew Neil
Super User
March 18, 2025
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
fa31Author
Associate III
June 17, 2025

Hi,

I used SPI3 to talk to the WiFi module. I used PC10, PC11 and PC12 pins:

fa31_0-1750160205453.png

 

My WiFi related main code is:

#include "main.h"
#include "b_l475e_iot01a2.h"

WIFI_HandleTypeDef hwifi;

int main(void)
{
 HAL_Init();
 SystemClock_Config();
 MX_GPIO_Init();
 MX_DFSDM1_Init();
 MX_I2C2_Init();
 MX_QUADSPI_Init();
 MX_USB_OTG_FS_PCD_Init();

 BSP_COM_Init(COM1); // Enable UART for logging
 BSP_SPI3_Init(); // Initialize SPI

 wifi_configs(&hwifi); // Configure WiFi
 wifi_join_network(&hwifi); // Join WiFi network

 while (1)
 {
 // application
 }
}
 
Hope it helps!