Wiring of VLXSMPS and VDDSMPS pins on STM32U575xx when SMPS is not used?
I am referring to the note AN5373 and MB1550/1549 schematics to design a STM32U575xx based board. The note AN5373 shows no connection for the VLXSMPS and VDDSMPS pins when SMPS is not used. Do i just leave them floating? How should I connect them if I do not want to use the SMPS? Also there is no 'VCAP' pin on my symbol.
Please Assist.