Skip to main content
Associate II
September 1, 2024
Solved

x-stm32mp-gnss2 and stm32 nucleo-144 interface compatibility

  • September 1, 2024
  • 3 replies
  • 1395 views

Hi,

Recently, I purchased a X-STM32MP-GNSS2 Evaluation board which came with an antenna. As per the instructions, I could find its compatibility with STM32MP157F-DK2 and Raspberry Pi. 

Can anybody help me getting its interface and data logging using STM32 Nucleo-144 board? 

 

Best answer by STTwo-32

Hello @jitusanwale and welcome to the ST COMMUNITY :smiling_face_with_smiling_eyes:.

This shield is made to work and be compatible with Microprocessors. So, it is not compatible with Nucleo 144 that is used as an evaluation board for the STM32 Microcontrolers. If you want to use GNSS2 with an MCU, youmay have to use the https://www.st.com/en/ecosystems/x-nucleo-gnss2a1.html

Best Regards.

STTwo-32 

3 replies

STTwo-32
STTwo-32Best answer
Technical Moderator
September 1, 2024

Hello @jitusanwale and welcome to the ST COMMUNITY :smiling_face_with_smiling_eyes:.

This shield is made to work and be compatible with Microprocessors. So, it is not compatible with Nucleo 144 that is used as an evaluation board for the STM32 Microcontrolers. If you want to use GNSS2 with an MCU, youmay have to use the https://www.st.com/en/ecosystems/x-nucleo-gnss2a1.html

Best Regards.

STTwo-32 

Associate II
September 1, 2024

Thanks for quick response.

Associate II
September 1, 2024

I have raspberry pi, could you please help me by providing some examples of Raspberry pi and X-STM32MP-GNSS2 interfaces and online resources if available.