32F413: Strange VCAP1/VCAP2 Behavior?
I'm debugging a hand-stuffed PCB that could have a component stuffing error I cannot discern. The board's artwork is a minor tweak on a prior known-good PCB using a 32F413 in the 100-pin package.
This board will not boot.
However, all VDD pins are at +3V as intended and the nRESET pin is high. VCAP1 and VCAP2 pins are equipped with their 2.2uF bypass caps and have ~+1.2 volts on them. The quartz crystal is oscillating.
Then strangely 3 seconds after application of VDD the voltage on both VCAP pins drops to zero and the crystal stops. nRESET remains high.
What would force the VCAP pins to collapse to VSS after 3 seconds?
TIA for any advice on this.