Question
32F429I-Discovery upgrade ST-Link firmware trick
Posted on May 23, 2014 at 00:05
Hello all!,
For everyone with an STM32F429I-Discovery board trying to upgrade the ST-Link firmware thru the ST-Link Utility version 3.4.0. If you don't see the DFU mode present message on connect and ST-Upgrade refuses to connect, do this to make it work properly:1. Jumper both Boot0 and Boot1.2. Plug in the ST-Link cable and the USB OTG cable.3. Run ST-Link Utility, and select ''Upgrade Firmware'' to start ST-Upgrade.4. Do not click on connect yet (it will fail almost every time). 5. Unplug the ST-Link Mini-B cable, leaving the USB OTG Micro-B cable attached.6. Wait for 6 seconds.7. Plug the ST-Link Mini-B cable back in.8. Wait another 6 seconds.9. Click the ''Connect'' button. You should now see the current firmware message.Now you can click the ''Upgrade'' button to update the firmware. #stm32f429 #dfu #discovery #st-link