70% of new boards (STM32L433RCT6) cannot program
We have new boards with STM32L433RCT6 as MCU and only 30% of boards can program with STM32CubeProgrammer. Other boards just cannot connect to ST-LINK. I have tried these:
1. Use "under reset" mode, not working
2. Use JTAG signals. The good board can be connected and the bad one still cannot.
3. Use UART bootloader with BOOT0 pull up. The good board can be connected and the bad one still cannot.
I have checked every pin of STM32L433RCT6, and found there is a 2Hz square wave on PB8, I disconnected external connection to PB8, and the square wave still there. If I press reset button, it will go to low. Is this normal?
Can anyone help me? I really appreciate any help. Thank you!