Skip to main content
Graduate
July 15, 2025
Solved

A camera for many kits?

  • July 15, 2025
  • 2 replies
  • 363 views

i whant to know if the B-CAMS-OMV is compatible with the 32F746GDISCOVERY, NUCLEO-N657X0-Q, and the STM32N6570-DK?

because i why didn't I find the specific connector data of the 3 kits regarding the camera,
And I want to know this one camera B-CAMS-OMV is good for me for the 3 different kits?

    This topic has been closed for replies.
    Best answer by QSHAO.1

    B-CAMS-IMS (at B-CAMS-IMX - Camera module bundle for STM32 boards - STMicroelectronics) should be supported by N6 Nucleo and DK. thanks!

    2 replies

    ST Employee
    July 22, 2025

    Both NUCLEO-N657X0-Q and the STM32N6570-DK supports camera module with CSI interface, so they are not compatible with B-CAMS-OMV which is designed to support DCMI interface.

    Based on 32F746GDISCOVERY schematic, B-CAMS-OMV should work with this board.

     

    Graduate
    July 28, 2025

    okey , i need a MIPI CSI-2 camera!...

    Finally, what models of camera modules do you recommend for my NUCLEO-N657X0-Q that is compatible with it in MIPI CSI-2 protocol and connector (Socket_FFC/FPC, 22pins, 0.5mm, RA, SMD, T=2mm) from my NUCLEO-N657X0-Q board?
    (because I have not found any compatible and connectable model with it in other forums)
    QSHAO.1Answer
    ST Employee
    July 29, 2025

    B-CAMS-IMS (at B-CAMS-IMX - Camera module bundle for STM32 boards - STMicroelectronics) should be supported by N6 Nucleo and DK. thanks!