Skip to main content
Visitor II
August 24, 2022
Question

About STM32F205VET6 and STM32F205ZET6

  • August 24, 2022
  • 2 replies
  • 1165 views

Post removed.

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    August 24, 2022

    Hello @TYUKI.1​ ,

    Could you please provide more details about your issue encounter with STM32F205ZET6 ?

    The STM32F205VETx is an LQFP100 package, and STM32F205ZETx is LQFP144 package.

    So, you should refer to the STM32F205xx Datasheet and check the GPIO, pin assignment.

    0693W00000SteLaQAJ.jpg 

    0693W00000SteLuQAJ.jpg 

    You can use STM32CubeMX to compare the part numbers.

    For that, this FAQ may help you: How to compare different STM32 part numbers using the cross selection tool of STM32CubeMX?

    Check also the STM32F20x Errata sheet, if you have the limitation as described in the doc.

    When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

    Imen

    TYUKI.1Author
    Visitor II
    August 24, 2022

    Thank you very much for teaching me many things.

    We wanted to be able to put both 100-pin and 144-pin components on the board, so we designed the board as shown in the attached document.

    I ran a pattern through the pins that had the equivalent functions of the 100-pin and 144-pin components, and dropped all unused pins of the 144-pin ones to ground.

    This prototype board uses the 144-pin one, and the firmware is the program that was used when the 100-pin one was used.

    regards,