About the USB trace impedance needs in device mode
I'm referring to USB hardware and PCB guidelines using STM32 MCUs (AN4879)
and to USB 2.0 specification. MCU is STM32H755
In case when Embedded pull-up resistor on USB_DP line, USB 2.0 OTG HS controller with embedded on-chip HS PHYs and mode = device mode:
There (AN4879) were not mentioned about the USB DP or DM impedance or clearance needs, referred only to USB specification. In addition nothing in AN4938. Some manufacturers gives their recommendations to high-speed PCB designs, including USB for some materials. But not found any ST's document about that(?)
- So the general USB 2.0 high-speed rate differential trace impedance 90 Ω +/- 15% is correct?
I ask because think to need some confirmation before the implementation. Thanks in advance.