Accessing multiple wiznet modules using address bus decoding and single FMC SRAM nterface.
I have a requirement to interface 8 numbers of Wiznet Modules (Wiz830MJ) with STM32L496. Since i need to interface more than 4 modules so i cannot manage with standard FMC SRAM interface. So I am planning to use a decoder (74HC138D) and generate 8 different CS for modules. Please see the attachment. Remaining interface is same as standard FMC SRAM interface.
Kindly provide a feedback on this approach. If you see any issue then kindly highlight it.