Achieve max timer clock on STM32H7
Hello,
I am trying to achieve the maximum timer clock on the STM32H723ZG for input capturing. In the data sheet is written under Table 4: "The maximum timer clock is up to 550 MHz depending on theTIMPRE bit in the RCC_CFGR register and D2PRE1/2 bits in RCC_D2CFGR register."
I tried to achieve this in the Clock Configuration but it seems like the only solution I found is invalid (see screenshot below). Can I still do that? Or is there another way to do that?
I tried to compile it and it worked without a problem. Sadly I cannot test it on hardware due to delivery.
Thanks in advance!