Skip to main content
Visitor II
September 16, 2022
Question

Am working on NUCLEO STM32F401RE , so after debugging the code, am facing this issue. Please advise for this, so i can work speedy. Target no device found Error in initializing ST-LINK device. Reason: No device found on target.

  • September 16, 2022
  • 1 reply
  • 797 views

STMicroelectronics ST-LINK GDB server. Version 7.0.0

Copyright (c) 2022, STMicroelectronics. All rights reserved.

Starting server with the following options:

    Persistent Mode      : Disabled

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled

    SWD Debug         : Enabled

    InitWhile         : Enabled

Target no device found

Error in initializing ST-LINK device.

Reason: No device found on target.

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    September 16, 2022

    Hallo @kabid.1​ ,

    I advise you to refer to this FAQ: How to solve debugger connection issues.

    Check if all jumpers are correctly configured.

    Try using latest release of STM32Cubeprogrammer, and make sure to upgrade the ST-LINK/V2-1 firmware.

    Try connect to "Under reset" mode.

    When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

    Imen