B-G474E-DPOW1 debug using Tag-connector CN10 not working
Hi,
I have started working with the B-G474E-DPOW1 (STM32G474RE). The intention is to use the G474 in a custom design.
I can connect and use the board fine with the on-board debugger, but I want to use the TAG-Connector 10-pin header (CN10, as this is the plan for the target board later), but the connection is not recognised in the STM32CubeProgrammer. Programmer output::
13:36:00 : UR connection mode is defined with the HWrst reset mode
13:36:00 : ST-LINK SN : 39FF6.....
13:36:00 : ST-LINK FW : V2J45S7
13:36:00 : Board : --
13:36:00 : Voltage : 0.06V
13:36:00 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
I have followed the steps in the UG to disable the on-board STLINK-V3E (Section 9.2 STLINK-V3E physical disconnection) and I am using an external ST-LINK/V2 ISOL with a Tag-Connect adapter and cable (TC2050-ARM2010 adapter and TC2050-IDC cable)
- JP6 - Connected, STLK NRST -> Gnd
- SW1, Octal, all inactive i.e. switches up
- JP7 - removed
- Board powered with CN3 and LD6/LD7 lit, as expected
Do I need to do something else or have I misunderstood something to allow me to debug in this way?
Many thanks in advance for any help provided